Technical FAQs

Ask a Question

Can a QOU260 be used in place of a QOU260RP?

Issue:
Product features

Product Line:
QOU Unit mount breakers

Environment:
substitution

Cause:
Application

Resolution:
Yes. suffix 'RP' just means Retail Package. The breakers are the same.


CTA-ID : 2030467
Was this helpful?
What can we do to improve the information ?