Technical FAQs

Ask a Question

What type fuse is required for the 8538SD*12/22/62/65 Combination Starter?

This device is configured from the factory to accept Class H, J, K or R fuse types. However, this device is not supplied with Class R rejection pins. If Class J type (applications above 250 volt) fuses are used it will require re-positioning of the fuse base.

CTA-ID : 2030450
Was this helpful?
What can we do to improve the information ?