Technical FAQs

Ask a Question

Trying to install PowerSuite and is getting the following error and it will not install. ``Error 1325 ATV61_converter_de.dic, is not a valid short file name``. <br />

Need to install PowerSuite in another directory such as : ``C:\PowerSuite``

CTA-ID : 2030415
Was this helpful?
What can we do to improve the information ?