Technical FAQs

Ask a Question

What is the replacement for an HCM5074-8 I-Line panelboard interior?<br />

Use a HCM50918. It has the same amount of branch mounting space and will fit in the old 74`` high box. However, the original trim will not fit and there is no replacement trim available.


CTA-ID : 2030316
Was this helpful?
What can we do to improve the information ?