Technical FAQs

Ask a Question

What is meant by WITH NONVOLAT INI. or NO NONVOLAT INI.

 In STOP mode, when accessing the RUN/STOP menu, the interface proposes the following three choices for starting the program:

WITH NONVOLAT INI: All current values (counters, timers, etc.) are reset to zero before the program starts (default selection);
NO NONVOLAT INI: Current values for which the Latching option has been activated are kept;
NO: The program has not been started.

The navigation keys are used to change the selection. When the mode has been validated with the Menu/OK key, the display moves to the INPUT-OUTPUT screen.


CTA-ID : 2030277
Was this helpful?
What can we do to improve the information ?