Technical FAQs

Ask a Question

Cylinder lock and shunt trip combination: Is FAL34080CL1021 a legitimate Cat. No.?

Since 1021 is a left pole internal mounted shunt trip 120 - 240 Vac version, and CL is a left pole device, the Cat. No. Would need to be changed to reflect a right pole mounted shunt trip. Legitimate Cat. No. is FAL34080CL1001.

CTA-ID : 2029618
Was this helpful?
What can we do to improve the information ?