Technical FAQs

Ask a Question

Does the early-break switch 29345 mount inside the breaker or in the handle? Does it work with the door mounted handle?

It mounts in the handle assembly, not in the breaker. It will work with the door-mounted handle.

CTA-ID : 2029376
Was this helpful?
What can we do to improve the information ?