Technical FAQs

Ask a Question

Are Enclosures only, available for Meter Pak(MP) or EZM Metering Devices?

Issue:
Design repair parts

Product Line:
Meter Pak and EZM Metering

Evnironment:
Repair parts

Cause:
Maintenance

Resolution:
No. The Enclosures only for Meter Pak and EZM metering devices are not available. If a new enclosure is needed, the complete device will have to be replaced.


CTA-ID : 2029342
Was this helpful?
What can we do to improve the information ?