Technical FAQs

Ask a Question

What UL Standard and File are the Servicepak Power Outlet Panels (or PAK) Devices test and listed?

Testing and listing of EZM products

Product Line:
EZM Metering

UL Standards and Listing 

Customer request

The Servicepak Power Outlet Panels(or PAK Devices) are tested in accordance with standard UL 231. Additional UL standards may be referenced within the UL231 for compliance to that standard. The devices are UL listed in file #E53303.

CTA-ID : 2028954
Was this helpful?
What can we do to improve the information ?