Technical FAQs

Ask a Question

Can the HOM48L125GC Fixed main lugs load center, be converted to a main breaker load center?

Issue:
product features

Product Line;
Homeline load centers

Environment;
Convert to main breaker

Cause:
Application

Resolution;
This device is a Fixed Main Lug and is not convertible to a main breaker.

The only option to convert this panel to a main breaker load center would be to Back Feed a HOM, 2-pole branch breaker as the main. This would require a 2pole Homeline branch breaker rated less than the mains maximum rating and it would require the retaining kit catalog number HOM1RK. The Back-Fed option will use 2 of the load centers 4 spaces.

 
Was this helpful?
What can we do to improve the information ?