Technical FAQs

Ask a Question

Are NEMA 1 enclosures for NQ and NF panels available with welded endwalls, rather than bolt on type?

Issue:
Are NEMA 1 enclosures for NQ and NF panels available with welded endwalls, rather than bolt on type?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard enclosures sold and supported in the USA.

Cause:
Construction of panelboard enclosure endwalls.

Resolution:
NEMA 1 NQ and NF enclosures are not available with welded endwalls.








CTA-ID : 2029261
Was this helpful?
What can we do to improve the information ?