Technical FAQs

Ask a Question

What is the part number for ATV58 FIPIO communication option?

There are two choices:
The part number VW3A58301U is a pre-configured option card for 1 to 100hp ATV58 TRX drives.
The part number VW3A58311 is a generic FIPIO option card for all ATV58 TRX and Type FVC drives.


CTA-ID : 2013705
Was this helpful?
What can we do to improve the information ?