Technical FAQs

Ask a Question

How is a QO120AFI wired to a single downstream receptacle load ?

The colored load power or `` hot `` wire to the receptacle is connected into the upper (front ) terminal, marked ``Load Hot (symbol)``, and the white load neutral wire is connected into the lower (back) terminal, marked ``Load Neutral (symbol)``, of the breaker . The white pigtail on the breaker gets terminated on the panel neutral bar . Refer to the instruction bulletin for proper wiring.


CTA-ID : 2029065
Was this helpful?
What can we do to improve the information ?