Technical FAQs

Ask a Question

What is the part number for the 115 VAC logic input option card for the Altivar 61 or Altivar 71 drive?

VW3A3101 is the part number for the 115 VAC adaptor.
This adaptor is used to connect 115 V AC logic signals to the logic inputs on the drive or an I/O extension card.
7 logic inputs with capacitive impedance at 60 Hz of 0.22 ìF are available for connecting the logic signals:
- Max. current: 200 mA
- Response time: 5 ms to change from state 0 to state 1, 20 ms to change from state 1 to state 0
- Logic state 0 for a voltage below 20 V, logic state 1 for a voltage between 70 V and 132 V
The power supply must be provided by a 115 V AC external power supply (min. 70 V, max. 132 V).

CTA-ID : 2029337
Was this helpful?
What can we do to improve the information ?