Technical FAQs

Ask a Question

Can you add a B phase bus bar in the field to a 120/240V 3phase NQOD442L400TFL panel with a B phase high leg?

Issue:
Can you add a B phase bus bar in the field to a 120/240V 3phase NQOD442L400TFL panel with a B phase high leg?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No, the B phase bus bar is already in the panel, however, there is an insulator over the B phase which prevents breakers from being added in the field.


CTA-ID : 2029328
Was this helpful?
What can we do to improve the information ?