Technical FAQs

Ask a Question

What is the replacement for a XVBC11 mounting base?

Issue:
What is the replacement for a XVBC11 mounting base?

Product Line:
Harmony Tower Lights

Environment:
All Products

Cause:
Product Features

Resolution:
The XVBC11 base is obsolete and replaced by a new device which combines the base with the support tube.
Support tubes are no longer sold or available as separate components.
XVBZ02: with support tube, 3.15``H (80mm)
XVBZ03: with support tube, 15.7``H (380mm)
XVBZ04: with support tube, 31.5``H (780mm)

Note that these new devices consist of a black plastic base and black colored aluminum support tube. If a standard aluminum color tube is preferred, add ``A`` to the end of the catalog number.
XVBZ02A: with support tube, 3.15``H (80mm)
XVBZ03A: with support tube, 15.7``H (380mm)
XVBZ04A: with support tube, 31.5``H (780mm)



CTA-ID : 2029324
Was this helpful?
What can we do to improve the information ?