Technical FAQs

Ask a Question

Does the SC12L200S accept tandem branch breakers?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Environment:
Branch breakers

Cause:
Accepting Tandem breakers

Resolution:
No, The SC12L200S does not accept any 1-pole branch breakers. The device will ONLY accept (6) full size HOM, 2-pole breakers and would be used as main breakers(or service disconnects).


CTA-ID : 2035398
Was this helpful?
What can we do to improve the information ?