Technical FAQs

Ask a Question

What size is the ground bus/cable used in Power Cast and Power Dry units.

The standard method of grounding is a continuous #2/0 ground cable. If bus is specified a short section of #2/0 is placed at the ends to provide a flexible link


CTA-ID : 2028827
Was this helpful?
What can we do to improve the information ?