Technical FAQs

Ask a Question

What is the lug range for the PBCF5A225TB ?

The phase lugs in the PBCFA225TB accept wires from #6 to 300kcmil.
The ground lug in the PBCFA225TB accepts copper wires from 2/0 to #10 and aluminum wires from 2/0 to #6.

CTA-ID : 2029024
Was this helpful?
What can we do to improve the information ?