Technical FAQs

Ask a Question

Is a deadfront furnished with panelboard interiors or does it have to be ordered separately ?

Deadfronts are included as standard with the interiors . Special deadfronts ( extensions)  are also provided  with  main lugs, main breaker ,  and sub-feed breaker kits .


CTA-ID : 2029209
Was this helpful?
What can we do to improve the information ?