Technical FAQs

Ask a Question

Can you wire a HOM220GFI in a single pole circuit application?

Yes just wire up using only the right pole of breaker for the one phase wire as this is on the test button side. Everything else is wired the same.

CTA-ID : 2028863
Was this helpful?
What can we do to improve the information ?