Technical FAQs

Ask a Question

Is the RGF36160 breaker with a micrologic trip unit ET1.0I considered a solid state breaker?

Yes it is. But it only has a fixed continuous amperage and an adjustable instaneous.


CTA-ID : 2028803
Was this helpful?
What can we do to improve the information ?