Technical FAQs

Ask a Question

Does the KC34150 breaker have an adjustable magnetic trip setting?

Yes, it has a dial type adjustable trip setting that is nominally 750 amps on the low side and 1500 amps on the high side. It can be adjusted by means of a flat head screw driver.


CTA-ID : 2029187
Was this helpful?
What can we do to improve the information ?