Technical FAQs

Ask a Question

What is the standard terminal lug data for the EZM3800TB Series M01 and are alternate lugs available?

Issue:
Product design features

Product Line:
EZM Metering equipment

Environment:
Main Lug wire sizes

Cause:
Application

Resolution:
The Standard terminal lug data (or wire range) for this device is:

The line and neutral main lugs will accept (4) 3/0 AWG to 500 kcmil Al/Cu conductors per phase.

The Alternate terninal lug data (or wire range) for this device is:
1) To accept (2) 1/0 AWG to 600 kcmil Al/Cu OR (4) 1/0 AWG to 250 kcmil Al/Cu conductors per phase and neutral order (3) MMLK250 lug kits. Each MMLK250 Lug kit contains (3) 2 barrel lugs for terminating (1) 600 kcmil or (2) 250 kcmil Max. conductors. Two lugs can be placed on each phase and neutral.

2) To accept (2) 1/0 AWG to 750 kcmil Al/Cu conductors per phase and neutral, order lug kit part number 7329696650. This kit includes replacement Phase and Neutral, L-Shaped connectors where each is supplied with two (2) 1/0 AWG - 750 kcmil AL/CU lugs per connector assembly. The kit is also supplied with new mounting hardware, a new cross bus barrier and Drive Pin fasteners to secure the new cross bus barrier.





 
Was this helpful?
What can we do to improve the information ?