Technical FAQs

Ask a Question

What is the `Mains` wire size for a QO124M100, single phase load center?<br />

QO124M100 accepts one (1) - #6 to 2/0 AWG/kcmil per phase, Aluminum or Copper.


CTA-ID : 2028798
Was this helpful?
What can we do to improve the information ?