Technical FAQs

Ask a Question

Are lugs included for Altivar 71 drives that have the bus bar terminations?

No. Lugs must be provided. There are no lug kits for these products.
See the attached installation guide for hole dimensions depending on the drive part number.
This answer applies to ATV71HD55M3X and larger and the ATV71HD90N4 and larger size drives. The smaller drives have wiring terminations that do not require lugs.


CTA-ID : 2029093
Was this helpful?
What can we do to improve the information ?