Technical FAQs

Ask a Question

What is the maximum voltage rating and fuse amperage on a busplug catalog number PQ4206G?

The maximum fuse amperage is 60A and the maximum voltage is 240V.


CTA-ID : 2029046
Was this helpful?
What can we do to improve the information ?