Technical FAQs

Ask a Question

Is a bus extension device (e.g. EZM3EXT) needed if an EZM branch unit is mounted to the left of an EZM main device?

Issue:
Product requirements

Product Line:
EZM Metering Equipment

Environment:
Bus Extensions

Cause:
Application

Resolution:

Normally not, but some utilities want additional spacing between the main and the tenant meters. For these situations, there are bus extensions available for 1-phase and 3-phase applications.
-For 1-phase applications, use EZM1EXT6 (6 wide) or EZM1EXT (12 wide).
-For 3-phase applications, use EZM3EXT6 (6 wide) or EZM3EXT (12 wide).

 
Was this helpful?
What can we do to improve the information ?