Technical FAQs

Ask a Question

What is the difference between XY2CE1C290 and XY2CE1A290?

``C`` means it has a silicone boot and can be used in -40 F (-40 degrees C) temperatures. The minimum termperatures listed are based on the absence of freezing moisture or water. The XY2CE1A290 can be used in -13 degrees F to +158 degrees (-25 degrees C to +70 degrees C) temperatures.

CTA-ID : 2029047
Was this helpful?
What can we do to improve the information ?