Technical FAQs

Ask a Question

Is the QO112L125GRB, main lugs load center, convertible to a `main circuit breaker` load center?

Yes, for a 125A main circuit breaker, order catalog # - QOM125VH. Lower ampere ratings can also be used, from 125 amp down to 50 amp.

CTA-ID : 2029134
Was this helpful?
What can we do to improve the information ?