Technical FAQs

Ask a Question

What is the length of the ZCE06 cat wisker?

From the centerline of the mounting holes to the end of the cat whisker is 5.6 inches or 142 mm.


CTA-ID : 2028770
Was this helpful?
What can we do to improve the information ?