Technical FAQs

Ask a Question

What tools are required and what is the torque value for mounting different lugs on a PG1200 circuit breaker? It has star type bolts on the back of its lugs.

Screwdriver, Pozidrivᆴ #2 or #3, or slotted; Socket Wrench, 7 mm internal hex; Torque Wrench, 5/16 in. or 8 mm. 190 in/lb is the torque value for the lug mounting screws.

CTA-ID : 2029040
Was this helpful?
What can we do to improve the information ?