Technical FAQs

Ask a Question

What does the suffix 2144 designate?

It designates a 24 v DC shunt trip and 1A/1B form C auxilary contact. The leads are 18 gage copper, silver coated, 19 strand, black, wire with teflon insulation. The suffix for same devices with standard wire is 1386.

CTA-ID : 2029194
Was this helpful?
What can we do to improve the information ?