Technical FAQs

Ask a Question

What are the replacement bulbs for ZB2BW06**** or ZB2BV6***?

Issue:
What are the replacement bulbs for ZB2BW06**** or ZB2BV6***?

Product Line:
22mm Push Buttons

Environment:
ZB2 22mm Push Buttons

Cause:
Identify part number      
                                              
Resolution:
Direct supply light module is rated up to 380 volts. For direct supply light modules use:
incandesent
DL1CB006 6 volt AC/DC
DL1CE012 12 volt AC/DC
DL1CE024 24 volt AC/DC
DL1CE048 48 volt AC/DC
DL1CE130 120 volt AC/DC
neon
NE51HRT-120V 120 volt AC/DC
NE51HRT-220V 220 volt AC/DC
NE51HRT-380V 380 volt AC/DC





CTA-ID : 2029178
Was this helpful?
What can we do to improve the information ?