Technical FAQs

Ask a Question

Can the hardware that secures the core & coil assembly to the base of a medium voltage dry type transformer be loosened?

Confirm the location of manufacturer by looking at the bottom of the nameplate attached to the transformer. If the nameplate states the transformer was manufactured in Bland, VA, the hardware can be loosened. If the nameplate states the transformer was manufactured in the U.S.A or in Monroe, NC, the hardware can not be loosened.


CTA-ID : 2028861
Was this helpful?
What can we do to improve the information ?