Technical FAQs

Ask a Question

What is the largest mushroom head 9001 SK operator that can ge mounted in the top located, single operator position of a 9001 SKYP pendant station?

A 1-5/8`` diameter mushroom head operator is the largest diameter operator than can be mounted in this position.


CTA-ID : 2028810
Was this helpful?
What can we do to improve the information ?