Technical FAQs

Ask a Question

Can an HOM2125, 125A branch breaker, be used in the SC2040M200S Combination Service Entrance Device?<br /><br />

The branch breakers that can be used in this device are 15-110A and 150-200A. The 125A breaker cannot be used. The 150 and 200 amp breakers can be used because they connect to the bussing via 4 connection points.

CTA-ID : 2028796
Was this helpful?
What can we do to improve the information ?