Technical FAQs

Ask a Question

Can dimmers be used to adjust the output of control transformers ?

Dimmers can be used but they should be potentiometer style. If an electronic dimmer is used, it must of a quality that does not impress a DC voltage onto the transformer, DC voltage will cause the transformer to overheat and burn out



CTA-ID : 2029140
Was this helpful?
What can we do to improve the information ?