Technical FAQs

Ask a Question

What is the part number for an auxiliary contact for NEMA Type S contactors & starters?

Issue:     
Identifying part number for auxiliary contacts for a NEMA contactor or starter

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Ordering auxiliary contacts for a NEMA contactor or starter

Resolution:
Class 9999SX6 for one normally open, 9999SX7 for one normally closed or 9999SX8 for one normally open and one normally closed. These contact units are externally mounted and are field convertible from normally open to normally closed. For additional auxiliary contact options see Auxiliary Contacts in the Class 9999 Accessories section of the current Digest.


CTA-ID : 2029054
Was this helpful?
What can we do to improve the information ?