Technical FAQs

Ask a Question

What is the part number of the Hub Closing (or plastic) cap for the hub opening on the C200RB Series M01 Combination Service Entrance Device?

Issue:
Previous design repair parts

Product Line:
Combination Service Entrance Devices

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The part number for the Hub closing cap is BCAP, and the mounting screw is part number #2142720241. The BCAP requires two screws.


CTA-ID : 2029037
Was this helpful?
What can we do to improve the information ?