Technical FAQs

Ask a Question

Does the QO112M100RB come with a main circuit breaker?

YES. This is a convertible load center that comes with a factory installed main circuit breaker. The `M` in the Catalog # indicates that a main circuit breaker is Included from the Factory.

CTA-ID : 2028909
Was this helpful?
What can we do to improve the information ?