Technical FAQs

Ask a Question

Can an FA type circuit breaker with a GFM100FA ground fault module fit into an HCN I-Line panel?

No. You must use at least an HCP type panel to fit the GFM module into it, since the module adds 4.85`` to the length of the breaker.


CTA-ID : 2028889
Was this helpful?
What can we do to improve the information ?