Technical FAQs

Ask a Question

Do we have a lockout attachment for the stop button on a 9001BW240 to make it function like a 9001BW241?

No, but you can replace the cover on the 9001BW240 with a 9001BWD220 which is the cover from a 9001BW241, and it has the lockout on it.

CTA-ID : 2028831
Was this helpful?
What can we do to improve the information ?