Technical FAQs

Ask a Question

Can a PGA breaker be padlocked off when using a motor operator attachment?

Yes. The padlock attachment is included with the motor operator.


CTA-ID : 2029223
Was this helpful?
What can we do to improve the information ?