Technical FAQs

Ask a Question

What are the changes made on the FFTK firmware rev 1.1 versus the older rev 1.0?

The changes are primarily for functional improvement and fixing some bugs. Highlights are:
ᆱ Allows testing of the ET 1.0 trip unit on the Powerpact M frame breaker
ᆱ Provide integrated Screen Calibrator software
ᆱ Fix bugs (trip curves/time, error messages, translation issues, etc.)

The new firmware rev 1.1 can be downloaded (free of charge) from or websites using the following path: and resources/free software/Full-function Test Kit Firmware Rev 1.1

CTA-ID : 2029649
Was this helpful?
What can we do to improve the information ?