Technical FAQs

Ask a Question

Are AB1B6100 markers available marked with numbers higher than 100?

AB1B6 - 6mm markers go from 1 to 200:
AB1BV6 - blank
AB1B610 - marked 1 to 10
AB1B620 - marked 11 to 20
AB1B630 - marked 21 to 30
AB1B640 - marked 31 to 40
AB1B650 - marked 41 to 50
AB1B660 - marked 51 to 60
AB1B670 -marked 61 to 70
AB1B680 - marked 71 to 80
AB1B690 - marked 81 to 90
AB1B6100 - marked 91 to 100
AB1B6110 - marked 101 to 110
AB1B6120 - marked 111 to 120
AB1B6130 - marked 121 to 130
AB1B6140 - marked 131 to 140
AB1B6150 - marked 141 to 150
AB1B6160 - marked 151 to 160
AB1B6170 - marked 161 to 170
AB1B6180 - marked 171 to 180
AB1B6190 - marked 181 to 190
AB1B6200 - marked 191 to 200



CTA-ID : 2028845
Was this helpful?
What can we do to improve the information ?