Technical FAQs

Ask a Question

How do you order the 9003KAF1C cam switch operator with a custom engraved legend plate?

Soecify the desired marking and use the following part numbers to indicate the custom engraving.
9003KAF1C399 is how you would order this with a 30 degree switching angle/marking and get a custom engraved legend plate.
9003KAF1C499 is how you would order this with a 45 degree switching angle/marking and get a custom engraved legend plate.
9003KAF1C699 is how you would order this with a 60 degree switching angle/marking and get a custom engraved legend plate.
9003KAF1C999 is how you would order this with a 90 degree switching angle/marking and get a custom engraved legend plate.



CTA-ID : 2028773
Was this helpful?
What can we do to improve the information ?