Technical FAQs

Ask a Question

What is the power supply frequency in the Zelio relay at 100-240Vac? <br />

The operating frequency of the SR2/3 module with AC voltage is about 50 - 60 hz.
for a 50Hz network, the limits are 47 - 53Hz and for a 60Hz network, the limits are 57 - 63Hz.



CTA-ID : 2029559
Was this helpful?
What can we do to improve the information ?