Technical FAQs

Ask a Question

Is a PAK61PG Servicepak Power Outlet Panel provided with space for additional circuits to be field installed?

All receptacles and breakers are factory installed in this device. There is no space provided for additional circuits to be field installed.


CTA-ID : 2028765
Was this helpful?
What can we do to improve the information ?