Technical FAQs

Ask a Question

What is the Straight cable for a sensor with K suffix such as XS1M18MA230K<br /><br />Due to an error in SAP these do not follow the customary numbering convention. The correct <br />numbers appear on page 530 in the 9006CT0101 sensor catalog.**

Connector is a 3 pin female AC micro connector: [This now also applies to suffix ``U20``.]
XSZCK111Y Yellow PVC 2 meters
XSZCK112Y Yellow PVC 5 meters
XSZCK113Y Yellow PVC 10 meters
XZCP1865L2 Black PUR 2 meters
XZCP1865L5 Black PUR 5 meters
XZCP1865L10 Black PUR 10 meters


CTA-ID : 2028880
Was this helpful?
What can we do to improve the information ?